SLAU932 October 2024 AMC8V208
The AMC8V208EVM GUI uses I2C or SPI communication to control the AMC8V208. These functions are built into several GUI pages, as shown in the following subsections. The menu bar on the far left of the GUI allows the user to switch between pages. The menu bar displays the High Level Configuration page with the AMC Control subpage, and the Low Level Configuration page.
Before using the GUI, see the respective device data sheet for detailed AMC8V208 programming instructions.