SLDA058 March 2021 TUSS4470
Similar to the short range test, this measurement range was approximated and then four measurements were taken to show a progression towards the end of the range. The threshold method discussed above was used to compute the ToF on a single return echo pulse seen on VOUT. The threshold crossing is marked on the first plot.
This test shows a range up to about 0.895m. The full useful range for an application ultimately depends on the tolerable SNR and reliability of the measurement.