SLDA058 March 2021 TUSS4470
Figure 6-1 shows the TUSS4470 VOUT signal: undamped, 500Ω damped, and 75Ω damped, respectively. Cursors show the distance between the TX pulse and the first return echo pulse. To quantify the damping effect, cursor 'a' is placed to cross VOUT on the TX pulse approximately at the voltage level bisecting min and max of the leading edge of the first return pulse. Another helpful measure could be taken from the start of the TX decay until the first rising edge.
Figure 6-2 shows a 10 kΩ potentiometer soldered in parallel to the transducer across J3 on the TUSS4470EVM provided the adjustable damping resistance.
Figure 6-3 compares the constant ToF measurements, the damped measurements show a quicker decay before the first echo pulse arrives as the resistance is decreased. The timing metric used here also increases from 75.2 μs to 93.2 μs, illustrating that the minimum range will be somewhat improved with resistive damping. The drawbacks to resistive damping are reduced range or increased current consumption from the increased load on the transducer driver.