SLDA058 March   2021 TUSS4470

 

  1.   Trademarks
  2. 1Review of Ultrasonic Sensing Range Performance Factors
    1. 1.1 Physical Parameters
    2. 1.2 Transducer Characteristics
    3. 1.3 AFE Device Configuration
  3. 2Methods Overview
    1. 2.1 Introduction
    2. 2.2 Hardware Configuration
      1. 2.2.1 Transducers
      2. 2.2.2 Experimental Setup: Air-Coupled Level Sensing
      3. 2.2.3 Experimental Setup: Water-Coupled Level Sensing
      4. 2.2.4 TUSS4470 EVM Hardware Configuration
      5. 2.2.5 TDC1000-C2000EVM Hardware Configuration
    3. 2.3 Firmware Configuration
      1. 2.3.1 TUSS4470 Power Configuration
      2. 2.3.2 TUSS4470 220 kHz Configuration
      3. 2.3.3 TDC1000 220kHz Configuration
      4. 2.3.4 TDC1000 220kHz Configuration
      5. 2.3.5 TDC1000 1 MHz
  4. 3Short Range Air-Coupled Test Results
    1. 3.1 TUSS4470
    2. 3.2 TDC1000
  5. 4Mid-Range Air-Coupled Test Results
    1. 4.1 TUSS4470
      1. 4.1.1 Concept
      2. 4.1.2 TUSS4470 35 V Results
    2. 4.2 TDC1000
  6. 5Short Range Water-Coupled Test Results
    1. 5.1 TUSS4470
    2. 5.2 TDC1000
  7. 6Resistive Damping Device Comparison
    1. 6.1 TUSS4470
    2. 6.2 TDC1000
  8. 7Summary
  9. 8References
  10.   A Appendix A
    1.     A.1 TUSS4470: Filter Capacitor Selection
    2.     A.2 TUSS4470: Shematic
  11.   B Appendix B
    1.     B.1 TDC1000 Misc.
    2.     B.2 TDC1000-C2000EVM Schematic

TDC1000

Five measurements were taken, each with decreasing range (increasing water level), represented by separate colors shown in Figure 3-2. The COMPIN signal was probed with an oscilloscope and the data below is overlayed for each measurement. The START and corresponding STOP pulses are shown below the COMPIN plot. STOP pulses are corresponding in time with their respective COMPIN return echo. COMPIN signals are overlayed for visual comparison, and the data is trimmed after the return pulse to avoid visual data overlap. The START pulse is at time t=0 in yellow.

GUID-20210310-CA0I-RLB2-ZT3W-H1XSTQV06W3F-low.png Figure 3-2 Short Range Air-Coupled Results: TDC1000

In the TDC1000 short measurement mode, the minimum range is determined directly by the burst pulse time, blanking time, and TX ringing decay time. The blanking time is set to delay the listen period until just after the transducer ringing falls below ECHO_QUAL_THLD. The above results show that the blanking time was set to delay the listen period until approximately 175 μs, determined such that false STOP pulses triggered by ringing noise would be avoided. Notice that the pink and teal COMPIN signals both are measured at the beginning of the listen period and have a flat leading edge envelope compared to the other data. This happens when the return pulse is partially cut off by the blanking period. A partial echo such as this must be discarded because it does not represent the true ToF. To ensure a true measurement, some margin between the blanking period end and the minimum ToF measurement may be needed. Discarding the last measurement here, the minimum ToF accurately measured with this setup was at a 3.3cm distance from water level to transducer.