SLDA058 March 2021 TUSS4470
The water level in a small acrylic tank was adjusted for four measurements of decreasing water level. The 1 MHz Steminc transducer was used as described in Section 2.2. At this transducer frequency, using an oscilloscope to view VOUT is recommended over the MSP430F5529LP ADC and GUI display.
The ToF was computed in post processing using a threshold comparison on the TX pulse and first received echo shown on VOUT. Subsequent echo pulses show the decaying ultrasonic echo reflection, also seen in the short range air-coupled data. The minimum deletable water level with this method was 4cm.