SLLA579 January 2022 ISOUSB211
In the previous sections, the trace is either located upstream or downstream of the ISOUSB211 isolated repeater. Hence, we use either receiver equalizer or transmitter pre-emphasis to compensate for the trace loss. For a system that has a trace differential loss greater than 2 dB, it is recommended to distribute the loss to the upstream and the downstream of the ISOUSB211 and use the receiver equalizer and the transmitter pre-emphasis to compensate for the trace loss simultaneously. Figure 6-1 shows ISOUSB211EVM located between the FR-4 traces. In this setup, the receiver equalizer and the transmitter pre-emphasis work together to compensate for the total trace loss; the receiver equalizer compensates for the upstream trace loss, and the transmitter pre-emphasis compensates for the downstream trace loss.