SLLA621A September 2023 – October 2023 MCF8315A , MCF8316A
For sensorless FOC, since MCF831x has no sensors to provide position information, the startup is divided into the following steps: motor start-up , open loop, and hand off, close loop. Dividing the startup is because there is a complicated start-up process, but to make sure that each start-up link is executed correctly, so the start-up speed is not as fast as that of a brushed motor. However, we can take the time to optimize each step at the algorithm level and minimize the start-up time to be as short as possible.