One of the main applications that
utilizes multiprotocol transceivers are Industrial PCs (IPC, also known as single
board computers). Modern industrial manufacturing and automation have proliferated
IPC into multiple fields including factories, medical, automotive, and retail. Main
requirements for IPC design are:
- Robustness against transients to
support harsh industrial environment
- Communication versatility- IPC
needs to support large number of communication interfaces such as USB, Ethernet,
display port, RS-232 and RS-485
- Small form factor. High power
dissipation on board necessitates support for higher ambient temperature for
semiconductors used
There are pre-dominantly two ways a
multiprotocol transceiver is used by system designers:
- Single communication port needing
one interface at a time via shared bus/logic lines. So, the port is either a
RS-232 or a RS-422/RS-485 interface at one time. Main benefit for the
application is there is no need for two physical connectors- same connector can
be used as RS-232 or RS-485, so overall space needed on PCB is drastically
reduced.
- Two port requiring both
interfaces at the same time, but with each port configurable for either RS-232
or RS-422/RS-485.
These usage
methods are aimed towards mainly three application scenarios detailed below
- Shared port with on-the-fly
configurability: Certain applications need configurable communication
port. For example, an industrial equipment’s port is configured as RS-485 for
long distance multipoint communications. But during downtime, that port needs to
be converted to RS-232 for diagnostics or firmware upgrade. Multiprotocol
transceivers benefit such applications by requiring just one device instead of
having separate RS-232 and RS-485 transceivers. Additional discrete circuitry to
implement seamless switching between both interfaces and enabling/disabling
termination for either interface is eliminated as that functionality is now
integrated into the Multiprotocol transceiver, shrinking solution size
considerably.
- Single port fixed
interface: Multiprotocol transceivers comprising of RS-232 and
RS-422/RS-485 benefit the applications which just need one interface. Customers
can select, test and qualify multiprotocol transceiver, and configure it for
either interface. Main benefit is reduced development time and effort, and lower
inventory cost of management since now the customers do not have to select
different devices for different applications.
- Protocol translation:
Multiprotocol transceivers that enable both RS-232 and RS-485 interfaces
simultaneously can be used as protocol translator. Certain application scenarios
need an equipment’s legacy RS-232 port to be converted as RS-485 for long
distance communications. RS-485 inputs and outputs can be connected to RS-232
outputs and inputs to enable RS-232 communication distance extension.