SLLU173C October 2012 – September 2021 SN65176B , SN65HVD05 , SN65HVD06 , SN65HVD07 , SN65HVD08 , SN65HVD10 , SN65HVD11 , SN65HVD1176 , SN65HVD12 , SN65HVD1780 , SN65HVD1781 , SN65HVD1782 , SN65HVD1785 , SN65HVD1786 , SN65HVD1787 , SN65HVD1794 , SN65HVD20 , SN65HVD21 , SN65HVD22 , SN65HVD23 , SN65HVD24 , SN65HVD3082E , SN65HVD3085E , SN65HVD3088E , SN65HVD485E , SN65HVD72 , SN65HVD75 , SN65HVD78 , SN65HVD82 , SN65LBC176 , SN65LBC176A , SN65LBC182 , THVD1419 , THVD1429
All trademarks are the property of their respective owners.
TI RS-485 half-duplex devices in the 8-pin SOIC package have robust drivers and receivers in a small package for demanding industrial applications. The bus pins are robust to ESD events, with high levels of protection to Human-Body Model and IEC Contact Discharge specifications. These devices each combine a differential driver and a differential receiver, which operate from a single power supply. The driver differential outputs and the receiver differential inputs are connected internally to form a bus port suitable for half-duplex (two-wire bus) communication, and all feature a wide common-mode voltage range making the devices suitable for multi-point applications over long cable runs. TI's RS-485 devices are characterized for industrial applications.
This EVM comes without a transceiver soldered on to the board. The user can order any TI half-duplex, 8-pin SOIC RS-485 transceiver and solder it down on the board for evaluation. The EVM Tools Folder contains links to devices that work with this EVM. See http://www.ti.com/tool/rs485-hf-dplx-evm for more information.
Using the SN65HVD888 with Bus Polarity Correction Feature
This EVM can support the SN65HVD888 half-duplex RS-485 transceiver with bus polarity correction (See Figure 2-1). The SN65HVD888 transceiver corrects a wrong bus signal polarity caused by a cross-wire fault. In order to detect the bus polarity all three of the following conditions must be met:
After the failsafe time has passed, the polarity correction is complete and is applied to both, receive and transmit channels. The status of the bus polarity is latched within the transceiver and maintained for subsequent data transmissions.
Note: Data streams of consecutive 0’s or 1’s with durations exceeding tFS-min can accidently trigger a wrong polarity correction and must be avoided.
Figure 3-1 shows the schematic of the EVM. The EVM board has headers labeled from JMP1 to JMP14 (JMP5 is omitted) and two 3-pin terminal blocks labeled TB1 and TB2. These headers support device evaluation for a wide range of system configurations.
The examples in this document show a 3.3-V signal generator and a 3.3-V power supply unit. Depending on the Texas Instruments RS-485 device chosen, the user may need to provide a 5-V signal generator input and 5-V power supply.
For the first measurements, ignore the common-mode simulation and connect EARTH to GND through a wire-bridge between pin 1 and pin 2 of TB1.
While JMP2 to JMP4 are stimulation points, or headers through which the control and data signals for the RS485 Half-Duplex EVM are applied, JMP1, and JMP11 to JMP14 are probe points, or headers at which these signal can be measured.
Note that the 50-Ω resistors, R2, R3, and R4, have the index n.a., indicating that these components are not assembled. Because signal generators have a typical source impedance of 50 Ω, their output signal is twice the required signal voltage, and assumes that the on-board 50-Ω resistors divide this voltage down to the correct signal level.
Without these resistors; however, this voltage divider action is not accomplished, and the generator output voltage must be reduced to match the VCC requirements of the RS-485 device.
Figure 3-3 gives an example for entering a data signal into the driver section of the transceiver. The signal output of the generator is adjusted to match the device VCC power supply requirements . The generator’s ground terminal is connected with pin 3, and the signal output terminal with pin 2 of JMP4. The data signal is measured through an oscilloscope with its signal input connected to pin 1 and its ground wire connected to pin 2 of JMP14.
The same setup applies to the DE and RE inputs through their corresponding headers JMP2 and JMP12 and JMP3 and JMP13. JMP1 however, must not receive a signal stimulus. Like JMP11, it represents the receiver output, R, of the half-duplex RS-485 device.
Instead of using signal generators, the EVM can directly interface to the micro controller I/O. Then the non-assembled 50-Ω resistors are of no concern. However, for proper operation, it must be assured that the high-level input voltage VIH ≥ 2 V and the low-level input voltage VIL ≤ 0.8 V.
The generally recommended procedure for taking measurements is listed: