SLLU335A August 2021 – January 2022 MCF8316A
Acoustics is audible noise contributed by motor commutation and harmonic frequencies in motor drives. Stator excitation in motor drivers can generate mechanical resonance at audible frequency ranges leading to audible noise. Improving acoustic performance is important for applications that require quiet operation. Any distortion in phase current can translate to audible noise. Phase current distortion can be due to dead time, PWM modulation scheme or low MOSFET slew rate.
Step 1: Configure PWM Modulation scheme [PWM_MOD] to “Continuous Space Vector Modulation”.
In Continuous Space vector modulation, phase current waveform shaping will be better but the MOSFET switching losses will be higher.
In Discontinuous Space vector modulation, MOSFET switching losses will be lower. However, we can expect phase current distortion for low inductance motors.
Step 2: Enable Dead time compensation [DEADTIME_COMP_EN]
For speeds above 125 Hz, decrease MCC dead time [MCC_DEAD_TIME] till the phase current distortion gets better.
Decreasing the dead time might trigger Hardware lock detection current limit fault [HW_LOCK_ILIMIT]. If this fault gets triggered, increase the dead time.