SLLU338 August   2021 MCF8316A

 

  1.   Trademarks
  2. 1Cautions and Warnings
  3. 2Introduction
  4. 3Quick Start Guide
  5. 4Hardware and Software Overview
    1. 4.1 Hardware Connections Overview – MCF8316AEVM
    2. 4.2 Connection Details
    3. 4.3 MSP430FR2355 Microcontroller & User Interface
    4. 4.4 LED Lights
    5. 4.5 User-Configurable Settings
  6. 5Hardware Setup
  7. 6MCF8316A GUI Application
    1. 6.1 Running the GUI
    2. 6.2 Offline Installer
  8. 7MSP430FR2355 Interface Firmware
    1. 7.1 Downloading Code Composer Studio and Importing MSP430FR2355 Interface Firmware Code
    2. 7.2 Using the eZ-FET to Program the MSP430FR2355
  9. 8Schematics
    1. 8.1 Main Supply and Pi Filter
    2. 8.2 Connectors and Interface
    3. 8.3 USB to UART
    4. 8.4 MCU Programming and Debug
    5. 8.5 MSP430FR2355 MCU
    6. 8.6 MCF8316A 3-Phase Sensorless FOC Integrated Driver
    7. 8.7 Buck Regulator
    8. 8.8 Status LEDs
    9. 8.9 Switches and Speed Input
  10. 9Revision History

Downloading Code Composer Studio and Importing MSP430FR2355 Interface Firmware Code

  1. Extract the “MCF8316AEVM_MSP430FR2355_Firmware_GUI.zip” to a location on the computer.

  2. Download the latest version of Code Composer Studio. This will set up a ti folder in the directory C:\ti.

    1. Accept all agreements, default install locations, and hit “Next” to proceed through menus.

    2. In the “Select Components” window, ensure to check “MSP430 Low-Power MCUs” to install the required packages for the MSP430 LaunchPad Evaluation Kits.

  3. After installing, run CCS and select a folder or the default to use as the Workspace to store any new projects. The location and naming convention can be changed based on the user's preference. Click the OK button to accept.

  4. In CCS, click on the Project tab and select “Import CCS Projects”. Click on Browse.

  5. Select the “MCF8316AEVM_MSP430FR2355_Firmware_GUI” folder installed from step 1.

  6. Import the project “MCF8316AEVM_MSP430FR2355_Firmware_GUI” into your workspace as shown in Figure 7-1.

GUID-20210823-SS0I-PV51-8SRW-HGP1FLBXCGDW-low.pngFigure 7-1 MSP430FR2355 Interface Firmware Code in Code Composer Studio