SLLU338 August 2021 MCF8316A
The MCF8316AEVM has 5 status LEDs implemented that provide the status of power supplies and functionalities of the evaluation module. By default, the VM LED and 3.3 V Buck LEDs will light up when the board is powered and the program has been flashed onto the microcontroller. Table 4-1 shows LED descriptions including those that are on during power up in bold and Figure 4-5 shows the locations of the LEDs.
Designator | Name | Color | Description |
---|---|---|---|
D1 |
Buck Regulator |
Green |
Internal buck regulator is voltage output |
D2 |
nFAULT |
Red |
Lights up when fault condition has occurred on MCF8316A |
D3 |
ALARM |
Red |
Lights up when alarm condition has occurred on MCF8316A |
D4 |
VM |
Green |
Motor power is supplied to the board |
D5 |
MSP_LED1 |
Red |
Used for UART or debugging |
D6 |
MSP_LED2 |
Red |
Used for UART or debugging |