The eZ-FET Debug Probe on the MSP430FR2355 LaunchPad uses a SPI-by-Wire JTAG interface to program the MSP430FR2355 MCU on the MCF8316AEVM. Consult the MSP430 LaunchPad Development Kits for MSP430 LaunchPads that include an onboard eZ-FET Debug Probe.
- Remove the GND, 3V3, SBWTDIO, and SBWTCK jumpers from the MSP430 LaunchPad.
- Connect the top pins on the eZ-FET side of the
LaunchPad of the GND, 3V3, SBWTCK, and SBWTDIO signals to their respective pins
on J4 of the MCF8316AEVM as shown in Table 7-1 and Figure 7-2.
- Connect a micro-USB cable to the MSP430 LaunchPad and the PC.
- Click on the Build Project icon or “Ctrl” + B to ensure the project builds successfully. Accept any updates if needed from the Console.
- Click on Debug Project to set up a debug session and press the Play button to run the code.
- Stop the debug session, close Code Composer Studio, disconnect the SPI-by-Wire jumpers, and unplug the micro-USB cable from the MSP430 LaunchPad.
Table 7-1 SPY-BI-Wire Connections Needed to Program MSP430FR2355MSP430 LaunchPad™ (eZ-FET Debug Probe Side) (J101) | MCF8316AEVM 4-pin SPI-by-Wire Header (J4) |
---|
GND | GND |
3V3 | 3.3V |
SBWTDIO | SBWTDIO |
SBWTCK | SBWTCK |