The
following instructions assume the EVM is
configured for pin-strap mode and is powered from
J3 VBUS.
- Insert a Micro-B USB cable into J3 on the EVM.
Connect the other end of the USB cable to the
motherboard.
- Insert a USB device or USB cable into the lower
USB-A receptable of the EVM.
- The USB device should enumerate. If the USB
device does not enumerate, then check that VBUS is
at the appropiate level at D1 pin 1.
- Insert a Micro-B USB cable
into either J1 on the EVM. Connect the other end
of the USB cable to the motherboard.
- Insert a USB device or USB
cable into the upper USB-A receptable of the
EVM.
- The USB device should
enumerate. If the USB device does not enumerate,
then check that VBUS is at the appropiate level at
D2 pin 1.
The
following instructions assume the EVM is
configured for the I2C mode and is powered from
the barrel jack.
- Insert +5 V DC power source into the barrel jack
(J4).
- Configure the TUSB1004 through
the I2C interface (JMP1 and JMP2).
- Insert a Micro-B USB cable into either J3 or J1
on the EVM. Connect the other end of the USB cable
to the motherboard.
- Insert a USB device or USB
cable into either USB-A receptable of the EVM. Be
sure to connect that the USB device/cable into the
correposding USB-A receptacle (J3 = lower
receptaclce, J1 = upper receptacle)
- The USB device should enumerate. If the USB
device does not enumerate, check that VBUS is at
the appropiate level at the correcpsoding USB-A
receptacle, pin1 of D1 or D2.