SLOS438F December 2004 – March 2017 TPA2012D2
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
These typical connection diagrams highlight the required external components and system level connections for proper operation of the device. Each of these configurations can be realized using the evaluation modules (EVMs) for the device. These flexible modules allow full evaluation of the device in the most common modes of operation. Any design variation can be supported by TI through schematic and layout reviews. Visit e2e.ti.com for design assistance and join the audio amplifier discussion forum for additional information.
For this design example, use the parameters listed in Table 2.
PARAMETER | VALUE |
---|---|
Power supply | 5 V |
Enable inputs | High > 1.3 V |
Low < 0.35 V | |
Speaker | 8 Ω |
Temperature and applied DC voltage influence the actual capacitance of high-K materials. Table 3 shows the relationship between the different types of high-K materials and their associated tolerances, temperature coefficients, and temperature ranges. Notice that a capacitor made with X5R material can lose up to 15% of its capacitance within its working temperature range.
In an application, the working capacitance of components made with high-K materials is generally much lower than nominal capacitance. A worst-case result with a typical X5R material might be –10% tolerance, –15% temperature effect, and –45% DC voltage effect at 50% of the rated voltage. This particular case would result in a working capacitance of 42% (0.9 × 0.85 × 0.55) of the nominal value.
Select high-K ceramic capacitors according to the following rules:
The preceding rules and recommendations apply to capacitors used in connection with the TPA2012D2. The TPA2012D2 cannot meet its performance specifications if the rules and recommendations are not followed.
MATERIAL | COG/NPO | X7R | X5R |
---|---|---|---|
Typical tolerance | ±5% | ±10% | 80% to –20% |
Temperature | ±30 ppm | ±15% | 22% to –82% |
Temperature range (°C) | –55°C to 125°C | –55°C to 125°C | –30°C to 85°C |
The TPA2012D2 is a high-performance Class-D audio amplifier that requires adequate power supply decoupling to ensure the efficiency is high and total harmonic distortion (THD) is low. For higher frequency transients, spikes, or digital hash on the line a good low equivalent-series-resistance (ESR) ceramic capacitor, typically
1 µF, placed as close as possible to the device PVDD lead works best. Placing this decoupling capacitor close to the TPA2012D2 is important for the efficiency of the Class-D amplifier, because any resistance or inductance in the trace between the device and the capacitor can cause a loss in efficiency. For filtering lower-frequency noise signals, a 4.7 µF or greater capacitor placed near the audio power amplifier would also help, but it is not required in most applications because of the high PSRR of this device.
The TPA2012D2 does not require input coupling capacitors if the design uses a differential source that is biased from 0.5 V to VDD – 0.8 V. If the input signal is not biased within the recommended common-mode input range, if high-pass filtering is needed (see Figure 37), or if using a single-ended source (see Figure 38), input coupling capacitors are required.
The input capacitors and input resistors form a high-pass filter with the corner frequency, fc, determined in Equation 1.
The value of the input capacitor is important to consider as it directly affects the bass (low frequency) performance of the circuit. Speakers in wireless phones cannot usually respond well to low frequencies, so the corner frequency can be set to block low frequencies in this application. Not using input capacitors can increase output offset.
Equation 2 is used to solve for the input coupling capacitance.
If the corner frequency is within the audio band, the capacitors should have a tolerance of ±10% or better, because any mismatch in capacitance causes an impedance mismatch at the corner frequency and below.
For application curves, see the figures listed in Table 4.
For this design example, use the parameters listed in Table 2.
For the design procedure, see Detailed Design Procedure from the previous example.
For application curves, see the figures listed in Table 4.