SLOU583 September 2024 OPT101 , OPT3001 , OPT3001-Q1 , OPT3002 , OPT3004 , OPT3005 , OPT3006 , OPT3007 , OPT4001 , OPT4001-Q1 , OPT4003-Q1 , OPT4048 , OPT4060
Within the Latte scripts window, you can also send serial commands directly through the command line without having to open the GUI window. To send a command, simply use the syntax regProg._controller.sendPacket('command'), where 'command' is the specific instruction that you want to send. The full list of commands is shown in