SLOU583 September 2024 OPT101 , OPT3001 , OPT3001-Q1 , OPT3002 , OPT3004 , OPT3005 , OPT3006 , OPT3007 , OPT4001 , OPT4001-Q1 , OPT4003-Q1 , OPT4048 , OPT4060
To begin calibration using the LIGHTSOURCE01EVM, fix the EVM on to a mounting fixture. The EVM has a rail mount on the bottom, which can be used to screw the device on to the test setup. For more information on the dimensions of the mounting fixture, please refer to the Section 5.
Below is an example of a mounting fixture that can be used to fix the EVM in place.
The EVM can then be screwed on using the screws at the bottom such as in the figure below.