SLOU583 September 2024 OPT101 , OPT3001 , OPT3001-Q1 , OPT3002 , OPT3004 , OPT3005 , OPT3006 , OPT3007 , OPT4001 , OPT4001-Q1 , OPT4003-Q1 , OPT4048 , OPT4060
If you prefer not to use the LIGHTSOURCE01EVM GUI, you can easily control the device through serial commands using a terminal application using a terminal application like Tera Term. After connecting to the correct COM port, you can send specific commands to the device to perform various functions. This method offers an alternative for controlling the characteristics of the light source without needing to use the Latte software. See for the full list of commands