SLOU583 September 2024 OPT101 , OPT3001 , OPT3001-Q1 , OPT3002 , OPT3004 , OPT3005 , OPT3006 , OPT3007 , OPT4001 , OPT4001-Q1 , OPT4003-Q1 , OPT4048 , OPT4060
This section discusses how to operate the LIGHTSOURCE01EVM software. The GUI has a primary window that is used to configure and read from the LIGHTSOURCE01EVM, along with a scripts window that can be used to automate the function of the calibration light source. Basic GUI functionality and a description of the tabs are also presented in this section.