SLOU583 September   2024 OPT101 , OPT3001 , OPT3001-Q1 , OPT3002 , OPT3004 , OPT3005 , OPT3006 , OPT3007 , OPT4001 , OPT4001-Q1 , OPT4003-Q1 , OPT4048 , OPT4060

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specifications
  6. 2Quick Start Guide
    1. 2.1 Hardware Setup
    2. 2.2 Software Setup
      1. 2.2.1 Hardware Requirements
      2. 2.2.2 Software Installation
      3. 2.2.3 Launching the LIGHTSOURCE01EVM Software
      4. 2.2.4 Software Operation
        1. 2.2.4.1 LIGHTSOURCE01 GUI
    3. 2.3 LIGHTSOURCE01EVM Light Sensor Calibration
      1. 2.3.1 Mounting and Setup
      2. 2.3.2 Calibration Procedure
  7. 3Software
    1. 3.1 Scripts Window
      1. 3.1.1 Hidden IDE Window
      2. 3.1.2 devInit.py
      3. 3.1.3 mLightController.py
  8. 4Serial Commands
    1. 4.1 Latte Command Line
    2. 4.2 Terminal Application
    3. 4.3 List of Commands
  9. 5Hardware Design Files
    1. 5.1 CAD Drawings
  10. 6Compliance Information
    1. 6.1 Compliance and Certifications
  11. 7Additional Information
    1. 7.1 Troubleshooting
      1. 7.1.1 Microsoft Windows 7 Manual Driver Installation
    2. 7.2 Trademarks

Microsoft Windows 7 Manual Driver Installation

This section outlines the manual driver installation process. If the user is using Windows 7 or if the Windows device manager shows 2 USB Serial Devices under as other devices when the EVM is plugged in instead of COM ports as shown in Figure 7-1, then use the following steps. If two USB Serial Device devices show up as COM ports automatically (as is the case with Windows 10), then this section can be skipped.

LIGHTSOURCE01EVM LIGHTSOURCE01EVM on MicrosoftWindows 7 With Drivers Not
                    InstalledFigure 7-1 LIGHTSOURCE01EVM on Microsoft®Windows® 7 With Drivers Not Installed
  1. Open the device manager.
    LIGHTSOURCE01EVM
  2. Right click on USB Serial Device and select Properties.
  3. Click the Update Driver button.
    LIGHTSOURCE01EVM
  4. Click Browse my computer for driver software
    LIGHTSOURCE01EVM
  5. Click Let me pick from a list of device drivers on my computer.
    LIGHTSOURCE01EVM
  6. Select Show All Devices and click the Next button.
    LIGHTSOURCE01EVM
  7. Click the Have Disk button.
    LIGHTSOURCE01EVM
  8. Click the Browse button.
    LIGHTSOURCE01EVM
  9. Navigate to “C:\Users\<username>\Documents\Texas Instruments\Latte\projects\OPT3004\drivers” and select MSP430_CDC. Click the Open button.
    LIGHTSOURCE01EVM
  10. Click the OK button
    LIGHTSOURCE01EVM
  11. Select the first USB serial device and click the Next button.
    LIGHTSOURCE01EVM
  12. Click the Yes button.
    LIGHTSOURCE01EVM
  13. The driver now installs properly.
    LIGHTSOURCE01EVM
  14. Repeat this process (steps 1 to 13) for the second USB Serial Device. All steps are the same except for step 2 and step 11. In step 2, make sure to right-click the second USB Serial Device. Likewise, on step 11 make sure to select the second USB Serial Device when installing the driver as the following figure shows.
    LIGHTSOURCE01EVM
  15. When the driver is installed, the user sees the following message.
    LIGHTSOURCE01EVM
  16. The two USB Serial Device devices appear in the device manager under Ports (COM & LPT) as the following image shows.
    LIGHTSOURCE01EVM