SLUA450A January 2008 – November 2022 BQ27421-G1 , BQ27425-G2A , BQ27425-G2B , BQ27441-G1 , BQ27505-J2 , BQ27505-J3 , BQ27505-J4 , BQ27505-J5 , BQ27520-G4 , BQ27530-G1 , BQ27531-G1 , BQ27545-G1 , BQ27546-G1 , BQ27741-G1 , BQ40Z50 , BQ40Z50-R1 , BQ40Z50-R2
The gas gauge algorithm uses three types of information to calculate remaining capacity (DataRAM.Remaining Capacity( )) and full-charge capacity (DataRAM.Full Charge Capacity( )).
DataRAM.Full Charge Capacity( ) is defined as the amount of charge passed from a fully charged state until the voltage defined in DF.Terminate Voltage flash constant is reached at a given rate of discharge, after subtracting the reserve capacity (DF.Reserve Capacity).
Note that DataRAM.Full Charge Capacity( ) depends on the rate of discharge and is lower at higher rates and low temperatures because the cell I*R drop causes the Terminate Voltage threshold to be reached earlier.