• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Measuring the Bode Plot of D-CAP, D-CAP2, andD-CAP3 DC/DC Converters

    • SLUAAF4A may   2021  – april 2023 TPS51397A , TPS53318 , TPS53319 , TPS53353 , TPS53355 , TPS548A28 , TPS548A29 , TPS548B22 , TPS548B28 , TPS548D22 , TPS549B22 , TPS549D22 , TPS54J060 , TPS54J061 , TPS54JA20 , TPS54JB20 , TPS566235 , TPS568215 , TPS568230 , TPS56C215 , TPS56C230

       

  • CONTENTS
  • SEARCH
  • Measuring the Bode Plot of D-CAP, D-CAP2, andD-CAP3 DC/DC Converters
  1.   Abstract
  2.   Trademarks
  3. 1D-CAP Feedback Loop
  4. 2D-CAP Bode Plot Measurement Setup
  5. 3Bode Plot Measurements
  6. 4Transient Response Waveforms
  7. 5D-CAP2 and D-CAP3 Bode Plot Measurement Setup
  8. 6Measurement Tips
  9. 7Summary
  10. 8References
  11. 9Revision History
  12. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Measuring the Bode Plot of D-CAP, D-CAP2, andD-CAP3 DC/DC Converters

Abstract

The stability test is an important part of the evaluation of a DC/DC converter. If done properly, the Bode plot result can be a very quick and useful way to help you gauge the stability of the converter. In the absence of a theoretical analysis, use a network analyzer to measure the Bode plot and confirm the stability of the design. The control-loop gain, which can be plotted in a Bode plot, is a very good indicator of the stability of the DC/DC converter.

Trademarks

D-CAP is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

1 D-CAP Feedback Loop

DC/DC converters using D-CAP, D-CAP2, and D-CAP3 control architectures, referred to as D-CAPx in this report, became popular for their fast transient response with minimal output capacitance and their simplicity by eliminating external compensation components. The D-CAPx control architecture, a derivative of non-linear constant on-time control, poses a challenge for designers when measuring the control-loop gain. As Figure 1-1 shows, breaking the control loop is the proper technique for traditional linear control architectures, like voltage-mode control and current-mode control, where there is only one output feedback path. But when measuring the control-loop gain for D-CAPx architectures, a different approach is necessary. The D-CAPx control architecture has two direct output feedback paths as shown in Figure 1-2: one through the feedback resistor divider network Rup and Rlow, and the other through the direct current resistance (DCR) injection circuit Rp, Cp, and Cff. The D-CAPx control system does not have a high DC gain error amplifier like the traditional type II or type III compensator of current-mode or voltage-mode control architectures, where the FB pin is usually the negative input of the error amplifier. For D-CAPx converters, the FB pin is only one of the inputs of the PWM comparator. By leaving out one of the feedback path outputs of the measurement, the Bode plot measured using the setup in Figure 1-1 does not directly correlate to the transient response waveforms. To properly measure the loop-gain Bode plot, the loop breaking point must include both feedback paths, as Figure 1-3 shows.

GUID-20210510-CA0I-L1PN-THBN-K9FGKJ2MKPRN-low.jpg Figure 1-1 Voltage-Mode or Current-Mode Control-Loop Gain Setup
GUID-20210510-CA0I-KRMQ-Z18S-8VXRBGTVRWKZ-low.jpg Figure 1-2 Block Diagram of a D-CAP Regulator With an External DCR Injection Circuit
GUID-20210510-CA0I-R4TW-KL5C-WMZC1BSRQQVD-low.jpg Figure 1-3 Proper D-CAP Regulator Control-Loop Bode Plot Measurement Setup

2 D-CAP Bode Plot Measurement Setup

For D-CAPx regulators, the PWM modulation gain is determined by the falling slope of the triangular waveform formed at the FB pin by the DCR injection network and output-capacitor equivalent series resistance (ESR). The parasitic inductance and resistance along the injection cable and noise coupled into the wires distorts the triangular waveform at the FB pin, which renders a different PWM modulation gain than the regulator with an improper test setup. To preserve accuracy, a bypass capacitor, Cpass, is added in parallel to a 20-Ω resistor by forming a high-pass filter. The corner frequency is set lower than one-half of the switching frequency of the converter so that the triangular waveform at the FB pin during the testing remains similar to that during normal operation. A 0.22 µF capacitor is used for a converter switching at 500 Hz in this example. For most applications, the proper Cpass value would be from 0.1 µF to 0.47 µF. To minimize the effect on the system, the DCR injection capacitor, Cp, should be less than one-tenth of Cpass, as Figure 1-3 shows.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale