SLUAAF4A may   2021  – april 2023 TPS51397A , TPS53318 , TPS53319 , TPS53353 , TPS53355 , TPS548A28 , TPS548A29 , TPS548B22 , TPS548B28 , TPS548D22 , TPS549B22 , TPS549D22 , TPS54J060 , TPS54J061 , TPS54JA20 , TPS54JB20 , TPS566235 , TPS568215 , TPS568230 , TPS56C215 , TPS56C230

 

  1.   Abstract
  2.   Trademarks
  3. 1D-CAP Feedback Loop
  4. 2D-CAP Bode Plot Measurement Setup
  5. 3Bode Plot Measurements
  6. 4Transient Response Waveforms
  7. 5D-CAP2 and D-CAP3 Bode Plot Measurement Setup
  8. 6Measurement Tips
  9. 7Summary
  10. 8References
  11. 9Revision History

D-CAP Bode Plot Measurement Setup

For D-CAPx regulators, the PWM modulation gain is determined by the falling slope of the triangular waveform formed at the FB pin by the DCR injection network and output-capacitor equivalent series resistance (ESR). The parasitic inductance and resistance along the injection cable and noise coupled into the wires distorts the triangular waveform at the FB pin, which renders a different PWM modulation gain than the regulator with an improper test setup. To preserve accuracy, a bypass capacitor, Cpass, is added in parallel to a 20-Ω resistor by forming a high-pass filter. The corner frequency is set lower than one-half of the switching frequency of the converter so that the triangular waveform at the FB pin during the testing remains similar to that during normal operation. A 0.22 µF capacitor is used for a converter switching at 500 Hz in this example. For most applications, the proper Cpass value would be from 0.1 µF to 0.47 µF. To minimize the effect on the system, the DCR injection capacitor, Cp, should be less than one-tenth of Cpass, as Figure 1-3 shows.