SLUAAJ0 February 2024 TPS51397A , TPS54308 , TPS54320 , TPS54350 , TPS54538 , TPS54620 , TPS54622 , TPS54821 , TPS54824 , TPS563300 , TPS566231 , TPS566235 , TPS566238 , TPS568230 , TPS56C215 , TPS62933 , TPS62933F , TPS62933O
Figure 7-1 is a proposed design flow for PCM converter with second stage filter. All the inductance and capacitance used in calculation are effective value considering degrading.
To clarify, fcross≤fSW/10 for (Co+C2) calculation in Figure 7-1 is a conservative restriction to simplify the design flow. The bandwidth can be set higher according to actual conditions.
A design example is given with operating condition as: Vin=24V, Vout=1.2V, fsw=500kHz, Iout=3A. Targeted output ripple pk-pk amplitude Vo2-ripple-target is smaller than 1mV.
Based on the Equation 16 in TPS62933F data sheet, L=2.2uH is selected with K=0.345 (K is the ripple ratio of the inductor current: ΔIL / IOUT_MAX).
With Equation 26 for TPS62933F, we can get the lower limitation of (Co+C2) as 105.8uF by setting fcross=50kHz, which equals to fSW/10. This set bandwidth is also much larger than fZ-EA of TPS62933F 10.6kHz[5].
Pre-select Co=69uF (47uF+22uF) and C2=47uF. The estimated fcross is 45.6kHz with Equation 26.
Calculate L2 lower limit with equation 7 in Part I SLVAFD4: L2≥8.2nH.
Calculate L2 upper limit with Equation 24 in this application note: L2<109nH.
Here we select two ferrite beads for verification of both limits: BLE18PS080SN1 with 15.3nH@1MHz close to lower limit and BLM18SN220TN1 with 103.4nH@1MHz close to upper limit.
For the feedback network, firstly select R1=5kΩ and R2=10kΩ following equation (1) in TPS62933F data sheet. Using the tool in appendix A for making fZff > fcross, we can get Cff=620pF corresponding to fZff=48.3kHz for the case with L2=15.3nH, and Cff=470pF corresponding to fZff=47.4kHz for the case with L2=103.4nH.
Figure 7-2 to Figure 7-4 show the experimental verification results of the power design with BLE18PS080SN1. The ripple amplitude is within 1mVpp in Figure 7-3 and can satisfy the requirement. Figure 7-4 is the load transient waveform when changing output current from 0.75A (25% of 3A) to 2.25A (75% of 3A) with 2.5A/us slew rate, which shows the good loop response.
Figure 7-5 to Figure 7-7 show the experimental verification results of the power design with BLM18SN220TN1. With larger L2 value, the ripple amplitude is further reduced to within 1mVpp in Figure 7-6. Figure 7-7 is the load transient waveform when changing output current from 0.75A (25% of 3A) to 2.25A (75% of 3A) with 2.5A/us slew rate, which shows the good loop response. The details can be found in TI reference design 3.8V to 30V Input, 3A, 1.2V Low-Output-Ripple Power Supply With Second Stage Filter Reference Design.