SLUAAM4 December 2023 BQ76905 , BQ76907
In this example, the CUV (undervoltage) protection feature is enabled along with the default protections. This requires writing 0xE1 to RAM address 0x9024, shown in Figure 3-3. The checksum is calculated on the address and data (0x24, 0x90, 0xE1) and is the complement of the sum of these bytes. In this case, the checksum is 0x6A. The length includes the two bytes for device address and command address for a total length of 0x05.