SLUAAM4 December 2023 BQ76905 , BQ76907
Before writing RAM registers, the recommendation is to enter CONFIG_UPDATE mode to prevent settings from taking effect until all changes are made. See Table 3-2. SET_CFGUPDATE and EXIT_CFGUPDATE both follow the Subcommand format. In Figure 3-2, the SET_CFGUPDATE Subcommand is given by writing 0x0090 to 0x3E.
Command | Name | Description |
---|---|---|
0x0090 | SET_CFGUPDATE | Enters CONFIG_UPDATE mode. |
0x0092 | EXIT_CFGUPDATE | Exits CONFIG_UPDATE mode. This also clears the Battery Status()[POR] and Battery Status()[WD] bits. |