SLUAAN5 February 2023 TPS61376
#GUID-785F6A36-A203-4CC0-81D2-6D23A58D669E shows a load transient of 2 A for 1 ms waveform with an average input current limit set to 500 mA.
During the load transient, the voltage across the output capacitor drops rapidly. The power source is required to provide a large current to charge the capacitor to the target output voltage. The average input current limit function makes sure that the current is within the range allowed by the power source. Until the output capacitor voltage reaches the target output voltage, the charging phase ends.