The BQ7690x (which includes the BQ76905 and BQ76907) is a highly accurate and low power battery monitor and protector family with a host-operated cell balancing feature. This document describes how to use the cell-balancing function, how to increase the balancing current using external circuitry (FETs and BJTs), and systems considerations for the host-controlled balancing algorithm.
All trademarks are the property of their respective owners.
Battery cells are typically matched during the manufacturing of battery packs. Over time, an imbalance in the state of charge may develop between cells and reduce the overall capacity of the pack. Having a battery monitor with the capability of cell balancing allows longer battery life for the pack.
The BQ7690x supports passive cell balancing by bypassing the current of selected cells during charging or at rest, using the integrated or external bypass switches. For external bypass switches, the user could select between FET or BJT transistors. Balancing must be initiated and controlled manually from a host processor.
While balancing is active, there will be a current flowing into the cell input pins. In order to measure accurately, cell balancing needs to be disabled temporary while measuring the individual cells. Therefore, the timing for measurement of cell voltages and evaluation of cell voltage protections by the device is modified during balancing. The internal balancing FETs are disabled temporarily during each ADSCAN while the cell voltages and shared slot are being measured while cell balancing is active on a cell.
Cell balancing of a particular cell consists of enabling an integrated FET switch across the cell. The balancing current is determined by value of the input filter resistors selected when using internal balancing. Field Effect Transitors (FETs) or Bipolar Junction Transistors (BJT) can be used to increase the balance current in applications where the internal balancing current may not be sufficient.
Internal balancing, external balancing with N-channel FETs, and external balancing with BJTs are discussed in this section. Considerations for power dissipation and timing is also discussed.