SLUAAT7 January 2024 BQ25672 , BQ25790 , BQ25792 , BQ25798
If no PG pin is available, the charger is always bucking (for example. input voltage > battery voltage + PFET’s VGSth) and the maximum system (battery) voltage is below VGSmax-Q1, the input voltage can be used to directly drive the PFET’s gate, as shown in Figure 5-3.
The Zener diode clamp, D1, from the PFET’s source to gate is only necessary if the charger's input voltage is higher than the VSGmax-Q1. If this configuration, RPD provides current limiting for D1 in forward mode, for example, when no VBUS is applied.