SLUSCD1C June 2017 – November 2018 TPS2373
PRODUCTION DATA.
The APD pin is used in applications that may draw power either from the Ethernet cable or from an auxiliary power source. When a voltage of more than about 1.65 V is applied on the APD pin relative to RTN, the TPS2373 does the following:
This also gives adapter source priority over the PoE. A resistor divider (RAPD1–RAPD2 in Figure 30) provides system-level ESD protection for the APD pin, discharges leakage from the blocking diode (DA in Figure 30) and provides input voltage supervision to ensure that switch-over to the auxiliary voltage source does not occur at excessively low voltages. If not used, connect APD to RTN.
Note that RAPD2 must be no more than 200 kΩ.