SLUSCD1C June 2017 – November 2018 TPS2373
PRODUCTION DATA.
The waveforms of Figure 24 demonstrate detection, classification , and startup from a PSE with Type 3 Class 6 hardware classification. The key waveforms shown are V(VDD-VSS), V(RTN-VSS) and IPI. IEEE 802.3bt requires a PSE allocating Class 6 level of power to generate a minimum of two detection levels, four class and mark cycles, and startup from the fourth mark event. As shown below, the required minimum duration of the first class event has been extended for Type 3 and 4 PSEs. VRTN to VSS falls as the TPS2373 charges CBULK following application of full voltage. In Figure 26, assertion of the PG signal is delayed and used to enable load current as seen in the IPI waveform.