SLUSDG1C June 2020 ā August 2022 BQ25792
PRODUCTION DATA
After the REGN LDO powers up, the device checks the current capability of the input source. The input source has to meet the following requirements in order to move forward to the next power on steps.
Once the conditions are met, the status register bit PG_STAT is set high and the INT pin is pulsed to signal the host.
If VBUS_OVP is detected (failing condition 1 above), the device automatically retries detection once the over-voltage fault goes away. If a poor source is detected (when pulling IPOORSRC, the VBUS voltage drops below VPOORSRC), the device repeats poor source qualification routine every 2 seconds. After 7 consecutive failures, the device sets EN_HIZ = 1 and goes to HIZ mode. The device will remain in HIZ until either the adapter is re-plugged or the EN_HIZ bit is toggled, which will restart poor source detection with another 7 attempts. The EN_HIZ bit is cleared automatically when the adapter is plugged in. If either condition 1 or condition 2 is not met, it means the input source is not qualified; the PG_STAT bit remains low, and an INT pulse will be asserted and PG_FLAG will be set to 1, if PG_MASK = 0.