SLUSES3B October 2023 – July 2024 UCC25660
PRODUCTION DATA
UCC25660x family provides programmable brown-in and brown-out threshold. When the voltage on the BLK pin falls below VBLKStop, the controller enters brown out state and stops switching. In the brown-out state, an additional current sink is turned on to draw IBLKHys form the BLK pin. By changing the equivalent resistance connected to the pin externally, the actual brown-in voltage can be programmed.
When brown-out is detected, the controller stops switching. If BLK voltage rises above the brown-in voltage, the controller immediately begins soft start and does not wait for fault idle time.
In the variants that have the BLK OVP option enabled, if the BLK pin voltage rises above the OVP threshold, the controller stops switching and move to the fault state. After the fault idle time, the controller checks if the OVP condition is cleared. If the OVP condition is removed, the controller begins recovery and soft start. If the OVP condition is not cleared, the controller stays off and waits until the OVP condition is cleared.