SLUSFU9 October 2024 BQ51013C
PRODUCTION DATA
Figure 9-4 shows wireless power start-up when the RX is placed on the TX. In this case, the BQ500212A is used as the transmitter. When the rectifier voltage stabilizes, the output is enabled and current is passed. In this case, the load is resistive generating 900 mA. The pulses on the RECT pin indicate communication packets being transferred from the RX to the TX.
Figure 9-5 shows a current transition. The plot shows a 1-A load removed then added again. Note the stability of VOUT.