Figure 4-2 is the recommended test setup to evaluate the TPS53353EVM-744. Working at an ESD workstation, make sure that any wrist straps, bootstraps or mats are connected referencing the user to earth ground before power is applied to the EVM.
Input Connections:
- Before connecting the DC input source VIN, it is advisable to limit
the source current from VIN to 10-A maximum. Ensure that
VIN is initially set to 0 V and connected as shown in Figure 4-2.
- Connect a voltmeter V1 at TP1 (VIN) and TP2 (GND) to measure the
input voltage.
- Connect a current meter A1 to measure the input current.
Output Connections:
- Connect the load to J3, and set the load to
constant resistance mode to sink 0 A before VIN is applied.
- Connect a voltmeter V2 at TP5 (VOUT)
and TP7 (GND) to measure the output voltage.
Other Connections:
Place a fan as shown in Figure 4-2, and turn it on, ensuring that air is flowing across the EVM.