Use the following steps to enable the
EVM test setup.
- Make sure Section 2.2 steps
have been followed.
- Remove the shunt on JP17 to disable charge.
- Make sure the PROG pin
jumpers, JP22-JP29, are set to the desired frequency and cell count.
- Make sure the TS Jumpers are
installed to the correct posistions if a thermistor is being simulated.
- If using BQStudio, launch the
BQSTUDIO software and select Charger then BQ25792EVM, if not already
done.
- If using TI Charger GUI, go
to the TI Charger GUI website and select the charger
from the list.
- Turn on PS1 and Load #1:
- Measure ➡
VSYS-PGND (TP26 and TP48) = 8.55 V ±0.2 V
- Verify PG
LED (D13) is on.
Note:
If the PG LED is not lit,
confirm a valid PS1 is connected and the correct shunt configuration
was placed.
Note:
If the device is not communicating and does
not ACK, verify that Section 2.2
and the steps in this section have been followed. Verify the voltage
across TP42 (PULLUP) and TP49 (AGND) is approximately 3.3 V.