SLUUCI8 November 2023 BQ76905
The BQ76905 device integrates a special hardware block that monitors if the LFO stops oscillating or deviates significantly in frequency versus its expected value. If this is detected, the device immediately transitions into SHUTDOWN mode if Settings:Configuration:Power Config[LFOWD] is set. This check operates in DEEPSLEEP mode as well as NORMAL and SLEEP modes.