Enable supply #1, if the current on
DMM1 is more than 0.25 mA and less than 0.71 mA, everything is set
correctly.
Enable function generator outputs
channel-A and channel-B.
The following conditions should be
present:
Stable pulse output on
channel-1 and channel-2 in the oscilloscope, refer to #SLUUBM28383.
Frequency measurement
should be 100 kHz, ±5 kHz or equal to the programmed function generator
frequency.
DMM #1 should display
around 3.2 mA ± 1.5 mA with the default load capacitance of 1.0 nF. For
more information about operating current, see the LM2105 data
sheet.
Figure 5-1 Example Input and Output
Waveforms (green and magenta are PWM inputs, blue and dark blue are driver
outputs)