SLUUCT6 April 2024 BQ25186
To enter the Ship Mode state, connect the equipment as follows:
Turn ON power supply #2. Enter Ship Mode by setting the EN_RST_SHIP bits in the SHIP_RST register (0x09) to 2b10. Users are in Ship Mode when the voltage on SYS (SC #3) falls to 0V and the voltage on TS/MR (SC #4) still periodically pulses to monitor button press.
Alternatively, Ship Mode can be entered through a long button press. Turn ON power supply #2. With VSYS active (not in Ship Mode or Shutdown Mode), make sure that the PB_LPRESS_ACTION bits are set to 2b10: Enable shipmode. After holding the button SW1 for longer than MR_LPRESS (default: 2b01 (10s), the voltage on SYS (SC #3) falls to 0V.
To exit Ship Mode, hold the TS/MR button SW1 until VSYS enables. Turning on VIN at 5V also exits Ship Mode.