SLUUCT6 April 2024 BQ25186
Connect the equipment as follows:
Turn ON power supply PS #2, then turn ON supply PS #1. With PS #1 enabled, VSYS rises to the level of 4.5V and the /PG LED turns on to indicate Power Good. The device begins to charge as long as TS is left at default configuration, J13 connects the /CE pin to low, and there are no other faults.
To adjust the charge current or change other parameters, connect the USB2ANY to the EVM and then startup the TI Charger GUI.
Select BQ25186 from the charger selection. Click Quick Start or Register Map.
The quick start is shown in Figure 4-4. Disabling the charge through I2C overrides the charge disable pin.
The register map is shown in Figure 4-5.