SLUUCY9 November 2023 BQ76905
The Commands tab is displayed on the right side of the BQStudio window. Buttons in this tab allow reading various information about the device and certain operations by sending a command to the device. Commands and returned data are shown in the Log Panel of the tab. The seal function is unusual in general evaluation and is not recommended during initial evaluation.
Sealing the device without remembering the key reduces the function of the EVM.