SLUUCY9 November 2023 BQ76905
Features are controlled by commands as described in the BQ76905 data sheet. Data is available from registers, and the registers view shows data, but a user can send specific commands to the device. The Command sequences tool allows this operation and is shown in Figure 5-7. The Device Send and Receive section allows read or write to a single or consecutive locations. The Command Sequence section allows reads and writes to be intermixed in a sequence. Sequences can be stored to files or called from files. Files can be assigned to buttons in the Command Sequence File Assignment Buttons section. Results can be viewed in the Transaction Log and saved to a file if desired.