An external bias ranging 4.75V to 5.3V can be
connected to the VCC/VDRV pin. This connection enhances the efficiency of the converter
because the VCC/VRDV power supply current now runs from this external bias instead of the
internal LDO.
The following are considerations when using an
external bias on the VCC/VDRV pin:
- Connect the external bias to VCC/VDRV
pin.
- When the external bias is applied on the VCC/VDRV
pin earlier than PVIN rail, the internal LDO is always forced off and the internal analog
circuits have a stable power supply rail at the power enable.
- (Not recommended) When the external bias is
applied on the VCC/VRDV pin late (for example, after PVIN rail ramp-up), any power-up and
power-down sequencing can be applied as long as there is excess current pulled out of the
VCC/VDRV pin. Understand that an external discharge path on the VCC/VDRV pin, which can
pull a current higher than the current limit of the internal LDO, can potentially turn off
VCC/VDRV LDO, thereby shutting off the converter output.
- A good power-up sequence is: the external bias is
applied first, then the 12V bus is applied on PVIN, and then EN signal goes high.