Use the following instructions to verify the
startup behavior of LM74681.
- Set the input supply voltage to 48V and current
limit of 3A
- Make sure the J2 jumper setting is set to 2-3.
- Plug the positive end of power supply to J1 and
negative end to J2.
- Turn ON the power supply and observe the behavior
of TG1-IN1, BG1, and OUTP.
- Turn OFF the power supply and reverse the connection on J1 and J2.
- Turn ON the power supply and observe the behavior
of TG2-IN2 and BG2 with OUTP same as step 4.