SLVAE59A February 2019 – April 2022 DRV8242-Q1 , DRV8243-Q1 , DRV8244-Q1 , DRV8245-Q1 , DRV8343-Q1 , DRV8702-Q1 , DRV8702D-Q1 , DRV8703-Q1 , DRV8703D-Q1 , DRV8803 , DRV8804 , DRV8805 , DRV8806 , DRV8860 , DRV8873 , DRV8873-Q1 , DRV8874 , DRV8874-Q1 , DRV8876 , DRV8876-Q1 , DRV8935 , DRV8955
A solenoid is a coil that produces a linear or rotational movement in a mechanical system by applying a current through the coil. There are several types of solenoids, but generally their main use is to displace objects or maintain a specific state or position, much like a traditional relay. These electromechanical solenoids consist of a copper inductive coil wound around a steel or iron armature, sometimes called a “plunger”. The magnetic field of the energized coil pulls on the armature, and the armature transfers a mechanical force to an external mechanism.
Within each application, solenoids and relays are driven in different configurations. Some example solenoid applications include home appliances, printers, HVAC, irrigation systems, engine and transmission control.
This application report categorizes and describes a few types of solenoids, discusses driver configurations, and highlights semiconductor solutions from TI that can simplify solenoid driver solutions.