SLVAE87A December 2020 – October 2023 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
The BQ79616-Q1 can handle 240 mA max at 105°C. Should more current be needed, the cell balancing pins are able to support an external FET as shown in Figure 4-5. Cell balancing current with external FET can be calculated using equation below. Details for that configuration can be found in the BQ79616-Q1 data sheet.
There are a few things to keep in mind regarding external balancing. First, the series resistors between the FET and pin are there to protect the pins during hot plug and the capacitor is there to ensure that the FET does not turn on during hot plug. Also be aware of the following conditions that should be considered when selecting the FET.