SLVAE87A December 2020 – October 2023 BQ79600-Q1 , BQ79612-Q1 , BQ79614-Q1 , BQ79616-Q1 , BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
The device provides a dedicated bus bar channel through the BBP/BBN pins for bus bar connection and measurement. It is a “floating” channel allowing the bus bar to be connected to any cell except the bottom cell of a module.
Instead of using the BBP/BBN with the bottom cell (VC1-VC0), the bus bar could be connected to the BBP/BBN of the lower stack device alternatively as shown as Figure 5-1.
Using the bus bar channel maximizes the use of cell channels in the device across different module size. As described in Figure 5-2, 4 x 12 cell can be monitored by 3 CMC without wasting any pins while connecting the bus bar to BBP/BBN.