SLVAFD0B may 2022 – september 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , TPS65219 , TPS65219-Q1 , TPS65220
There are several considerations to take into account when designing the TPS65219 to power the AM62 processor and the peripherals.
Each of these questions impact the design, configuration, setup, among others, of the power block diagram and plays a role designing the most robust power solution. The sections below describe how the TPS65219 PMIC can supply the AM62x processor on different application requirements.
All the TPS65219 variants described in this application note have LDO1 configured as bypass to supply the SD card dual-voltage I/O (3.3 V and 1.8 V). A processor GPIO control signal with a logic high default value and an external pull-up is used to set SD IO to 3.3 V initially. After the power-up sequence, the processor can set GPIO signal low to select 1.8 V level as needed for high-speed card operation per SD specification. This bypass configuration allows control of the LDO1 voltage from 3.3 V to 1.8 V without the need to establish I2C communication during boot from SD card operations. The bypass configuration on LDO1 requires connecting its input supply pin (PVIN_LDO1) to 3.3 V.