SLVAFF1 January 2023 DRV8452 , DRV8462
PRODUCTION DATA
The power saving can be improved even further, if the ATQ_UL adapts to the maximum ATQ_CNT at each current level. This adaptive ATQ_UL can be implemented in firmware by continuously updating the value of ATQ_UL as a function of the motor current, as shown by the envelope plot in Figure 2-16.
With adaptive ATQ_UL, the current waveform in Figure 2-18 saves more power than the non-adaptive case shown in Figure 2-17.