SLVAFF1 January 2023 DRV8452 , DRV8462
PRODUCTION DATA
In this application, the stepper motor was subjected to load torque transients between 50 mNm and 1.5 Nm at a fast rate of 1.5 Nm/15ms. The on time for the peak load was roughly 1 s, and the duration between peak load events was 4 s, corresponding to a 20% duty cycle for the peak load.
Figure 3-6 shows the snapshot of the learning routine for this motor.
The auto torque learning routine was run at no load with the following parameter values:
Values for the ATQ_LRN parameters are:
The parameters for current control and PD loop control were selected as:
Figure 3-7 to Figure 3-10 showcase the output current and supply current waveforms with and without auto-torque in the event of a load torque change. As is expected, supply current consumption is significantly lower with auto-torque.
Based on lab measurements: